Windows Xp with w100 series.

Reply
Highlighted
Member
Posts: 3

Windows Xp with w100 series.

A friend suggested that if I were to intall windows Xp on my libretto it should work well with all of toshibas firmware, plus the added bennefit of less energy consumption. Culd someone verify this as truth?

Regular Advisor
Posts: 138

Re: Windows Xp with w100 series.

I really doubt you would have much success installing XP on the Libretto, XP is way to old to support the hardware (lack of SATA drivers). The Libretto was designed around WIndows 7. I've loaded Windows 8 on mine, but because of the resolution of the screens (1024x600) I'm unable to use the Windows 8 UI Applications.

Member
Posts: 2

Re: Windows Xp with w100 series.