11-16-2010 09:42 AM
Solved! Go to Solution.
11-17-2010 06:37 PM
Hey I have a question which dock model did you use and did it work with just one montor. I was think about getting a docking station for the libretto. Did you run video with the docking station and if so How did it work and did you play try any kind of video games. Let me know if you have any ideas on how to solve the docking station problem.
11-18-2010 03:44 PM
I have both the first and second generation of the DynaDock U, I have used them with multiple laptops and tablets and it works fine for a USB video card. I know some have used them for video and gaming, but I use them for productivity. Like I said, the video doesn't work properly on the Libretto W105 and is listed as not supported.
Sorry,
Jeff
11-22-2010 02:22 PM
It is weird...I tried the Toshiba Dynadock U at work and it didn't really work too well, but I just tried it on the same model at home and it worked. The only difference this time I only had the top screen active on the Libretto, using the bottom as the bulliton board and it installed fine...I guess I should eat my words above....
So the DynaDock U works, which should mean the DynaDock V should work as well...
Very Cool,
Jeff
12-12-2010 12:40 PM
12-12-2010 01:42 PM
I'm not worried about this, it is still a laptop video card...and I have never owned a laptop that can drive more than 2 monitors with the onboard card. The USB docking station has its own video card allowing you to drive the 3rd monitor. I know from past tablets that driving portrait mode is more demanding than lanscape which may explain my first experience.
Jeff
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.