01-30-2011 08:20 AM

01-30-2011 01:55 PM
Cute ![]()
01-30-2011 03:38 PM
I installed this yesterday and it looks like this may have helped the battery run-down problem when the PC is switched-off or hibernated. After leaving it overnight I still have 98% battery left, this seems to be a major improvement but will need to leave it for a few more days to make sure.
01-31-2011 09:55 AM
Thanks for the heads up.
Hope it is simple to do.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.