Re: New BIOS Posted

Reply
Regular Advisor
Posts: 138

New BIOS Posted

Hey All W100 and 105 owners...Toshiba US has posted a new BIOS. It has some major changes. I installed the night, so far so good...

Version 1.30 - 2011-01-26
•Improved Battery Management.
•Improved Deploy Center 5.5 recovery speed.
•Added support for the McAfee Endpoint Encryption eToken.
•Added support for the Paragon Backup & Recovery Suite.
•Implemented the INTEL specification for the Intel 5 Series Chipset to improve stability.
•Implemented the INTEL specification for the Intel Pentium U5400 Mobile Processor Series to improve stability.
Posts: 46,764
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: New BIOS Posted

Cute

-Jerry
Channel 9
Member
Posts: 4

Re: New BIOS Posted

I installed this yesterday and it looks like this may have helped the battery run-down problem when the PC is switched-off or hibernated.  After leaving it overnight I still have 98% battery left, this seems to be a major improvement but will need to leave it for a few more days to make sure.

 

 

Highlighted
Occasional Contributor
Posts: 11

Re: New BIOS Posted

Thanks for the heads up.  

 

Hope it is simple to do.