03-17-2011 11:57 AM
Is there a posibility to replace Libretto's 62 SSD drive with another SSD, with bigger capacity?
Solved! Go to Solution.
03-17-2011 07:11 PM
Its a MSATA drive so it should be possible, Toshiba has a 128GB Version in the same family as in the Libretto, model numer THNSNB0128GMCJ. I'm using a 32GB Micro-SD card for more storage personally...
02-20-2012 03:32 AM
I thought that the ssd was soldered ...
Am I wrong?
(I don't know how to open the w100 to exchange the ssd.)
02-20-2012 07:20 AM
This thread over at Pocketables shows how to open the case on the Libretto:
http://forum.pocketables.net/showthread.php?t=7378
On the pictures that show where to place the speaker, the rectangle right above the speaker looks to be the SSD. I could be wrong as I have not cracked the case of the Libretto, I used a 32GB MicroSD for more storage.
02-21-2012 04:09 AM
Thank you very much.
I also use micro-sd cards.
But some files need to be installed on the main "hdd".
Thank you also for the good pictures on how to open the w100.
But I can't recognize the ssd.
Can you confirm that it isn't soldered on the picture?
02-21-2012 06:59 AM
Sorry - I haven't cracked open the case of the Libretto. The Pocketables Member did to add stereo speakers. If you look at the picture with the Speaker, there is an orange rectangle that appears to be the SSD with the SATA connector...
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.