Reply
Member
Konpon96
Posts: 6
0
Accepted Solution

2 GB RAM(1,8 GB usable)

I have Libretto W100 with Windows Home Premium 32-bit. One day, I checked system information, and there is written, that my Libretto has 2 GB of installed memory, but only 1,8 is usable. Is this a problem or it's normal? Is there a possibility to make full 2 GB usable? I tried changing some functions in my HWSetup(full performance, CPU always high etc.) and changing from eco to balanced mode, but there is still 1,8 GB.

Ace Advisor
Jerry_Lippey
Posts: 33,424

Re: 2 GB RAM(1,8 GB usable)

So you have the model from Asia (specs attached)?

 

Yes, it's normal for Windows 7 not to make all the memory available.

 

   The usable memory may be less than the installed memory on Windows 7-based computers

-Jerry
Member
Konpon96
Posts: 6
0

Re: 2 GB RAM(1,8 GB usable)

I have W100-10D(with 3G), bought in Poland, probably imported from Great Britain.

 

Thanks for this link and info. :smileyhappy:

Ace Advisor
Jerry_Lippey
Posts: 33,424
0

Re: 2 GB RAM(1,8 GB usable)

 

So you have this one..

 

Libretto W100-10D ( PLW10E-00500FF3)

 

..whose software downloads are here.

 

You are welcome to post here, of course, but there are also European forums that may be of interest.

 

   Toshiba Support Forums in Europe

-Jerry