04-13-2011 02:43 PM
I have Libretto W100 with Windows Home Premium 32-bit. One day, I checked system information, and there is written, that my Libretto has 2 GB of installed memory, but only 1,8 is usable. Is this a problem or it's normal? Is there a possibility to make full 2 GB usable? I tried changing some functions in my HWSetup(full performance, CPU always high etc.) and changing from eco to balanced mode, but there is still 1,8 GB.
Solved! Go to Solution.
04-13-2011 04:52 PM
So you have the model from Asia (specs attached)?
Yes, it's normal for Windows 7 not to make all the memory available.
The usable memory may be less than the installed memory on Windows 7-based computers
04-14-2011 03:34 AM
I have W100-10D(with 3G), bought in Poland, probably imported from Great Britain.
Thanks for this link and info. ![]()
04-14-2011 11:21 AM
So you have this one..
Libretto W100-10D ( PLW10E-00500FF3)
..whose software downloads are here.
You are welcome to post here, of course, but there are also European forums that may be of interest.
Toshiba Support Forums in Europe
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.