1 - 10 of 10 posts
| Subject | Replies | Author | Kudos | Views | Solved Date/Time | |
|---|---|---|---|---|---|---|
|
|
I have Libretto W100 with Windows Home Premium 32-bit. One day, I checked system information, and there is written, that my Libretto has 2 GB of installed memory, but only 1,8 is usable. Is this a pr...
| 3 | 0 | 3292 | 04-14-2011 03:34 AM | |
|
|
Is there a posibility to replace Libretto's 62 SSD drive with another SSD, with bigger capacity?
| 5 | 0 | 3287 | 03-23-2011 08:11 AM | |
|
|
I decided to buy dual-screen Toshiba Libretto, but I have some problems with versions. Is there any difference between W100 and W105? Is the W100-10D that one with 3G and SIM card slot? Is the Japane...
| 2 | 0 | 2795 | 03-23-2011 08:11 AM | |
|
|
It is weird...I tried the Toshiba Dynadock U at work and it didn't really work too well, but I just tried it on the same model at home and it worked. The only difference this time I only had the top ...
| 2 | 1 | 2812 | 11-22-2010 08:22 PM | |
|
|
I'm happy to say I've solved my own problem with the Bluetooth software. All that's necessary is to manually force the Bluetooth device in Device Manager to use the Microsoft Generic Bluetooth Device...
| 2 | 0 | 4680 | 09-20-2010 04:59 PM | |
|
|
See this Toshiba explanation. 1.46GB partition and other small partition are for the System Recovery Options and the factory software image
| 3 | 3 | 3768 | 09-20-2010 04:58 PM | |
|
|
I got a headset but it seems I will need a mic also. Skypeing only works if a am right in front of the screen, which does no good if we are working on a variety of things. Any suggestions? I am g...
| 2 | 0 | 1413 | 09-20-2010 04:57 PM | |
|
|
I tried to sign up to be notified when the Toshiba Book Place goes live. I tried to input my email address with the standard keyboard layout. When I tried to enter the @ sign, I pressed the @+= key...
| 2 | 0 | 1695 | 09-15-2010 10:23 AM | |
|
|
Does anyone know if the libretto w100 will support Micro SDHC cards or only Micro SD?
| 2 | 0 | 1233 | 09-15-2010 10:21 AM | |
|
|
You have to set the View > Page Display option to "Two-up". I eventually went into the preferences menu and changed the default view to Two-Up for all documents.
| 0 | 1 | 1095 | 09-07-2010 09:00 AM |
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.