07-11-2012 11:30 AM
I have Satellite A665-S5186
Is it compatible with windows XP SP3 professional?
Thanks in advance.
07-11-2012 11:34 AM
it was running before on windows 7 (64-bit)
and now i want to install windows Xp sp3 (32-bit)
..............
07-11-2012 12:03 PM
Well, Sniper, I believe you could install XP as far as the machine is concerned but there is a very limited number of drivers and utilities available from Toshiba for XP on this machine. You can see them--12--at THIS SITE for your machine.
If you have a big enough HDD and insist on proceeding, why don't you partition your HDD and install the XP in the new partition and if you have any problems, your original Windows 7 will still be available. Type Disk Manage in the Start/Search box and click on Create and Format Hard Disk Partitions.
C.B.
P.S. Jerry Lippey, please step in here if I am the least bit misleading since you are the real expert on these matters.
07-11-2012 01:54 PM
Satellite L755-S5152 (PSK1WU-0RX048)
Best to upgrade Home Premium to Professional and then install XP Mode. Works really well here.
Upgrade to another edition of Windows 7 by using Windows Anytime Upgrade
Install and use Windows XP Mode in Windows 7
It's not necessary to have hardware vitualization enabled. See KB977206.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.