NO drivers for Satellite A215-SP6806 needed to downgrade to XP

Reply
Member
Posts: 1
Accepted Solution

NO drivers for Satellite A215-SP6806 needed to downgrade to XP

i need to downgrade my laptop Satellite A215-SP6806 to XP (any version), but i can´t find (OFFICIAL) drivers for my model, , I do not like Windows Vista I hope I can help find them, thanks

Posts: 46,819
Topics: 83
Kudos: 8,813
Solutions: 3,146
Registered: ‎12-04-2008

Re: NO drivers for Satellite A215-SP6806 needed to downgrade to XP

 

A215-SP6806 (PSAFGU-06301F)

 

 

You're in luck!

 

That model is in part-number family PSAFGU, which maps to PSAFGE for European machines.

 

Go to this European download site and look up the Satellite A210 with Short Model No. PSAFGE.

 

You'll find 31 drivers, utilities, and so forth for Windows XP.

 

You'll also find 30 drivers for 32-bit Vista in case they're needed.

-Jerry
Channel 9

View solution in original post


All Replies
Regular Advisor
Posts: 3,300

Re: NO drivers for Satellite A215-SP6806 needed to downgrade to XP

Have loads of patience with this tasking please. Recommendation is to put on a retail version of XP OS desired, no external components plugged in, and let the new Hardware wizard locate the devices. I would initially check present OS Device Manager and copy down manuf's name of devices or use BELARC Advisor template for assistance here,you will also need to go into the BIOS and reset the hard drive to 'compatability' mode for the SATA harddrive device. 

These have worked for some Toshiba users. Use in order posted please.

   ACHI XP F6 Install Tool for Windows XP 

   Intel Matrix Storage Manager

 

Here is some drivers for you:driver_wifi_realtek_os2009078a.exe,driver_modem_26470A.exe,

util_sd_memory_26023A.exe

Posts: 46,819
Topics: 83
Kudos: 8,813
Solutions: 3,146
Registered: ‎12-04-2008

Re: NO drivers for Satellite A215-SP6806 needed to downgrade to XP

 

A215-SP6806 (PSAFGU-06301F)

 

 

You're in luck!

 

That model is in part-number family PSAFGU, which maps to PSAFGE for European machines.

 

Go to this European download site and look up the Satellite A210 with Short Model No. PSAFGE.

 

You'll find 31 drivers, utilities, and so forth for Windows XP.

 

You'll also find 30 drivers for 32-bit Vista in case they're needed.

-Jerry
Channel 9