How To: Enter the system BIOS on Windows Vista and Windows XP computers

Started ‎09-05-2012 by
Modified ‎02-03-2015 by
(34,485 Views)

Toshiba Laptops

One or more of the following methods will be effective:

 

F2 key method

Turn the computer on. If you see an invitation to press the F2 key to enter Setup, do so. The Setup screen will appear. If this method does not work, repeat it, but hold F12.

 

Toshiba Hardware utility method

Run the Toshiba Hardware utility from the Toshiba Console. It may also accessible (as 'HWSetup') from the Windows Control Panel. Changes to some of the settings will require re-starting the computer. This method is the only way to access the BIOS settings on some notebook PCs (Satellite 5000 series, for example). (For these machines, pressing and holding the F12 key immediately after powering-on the notebook will allow you to alter the notebook's boot priority.) If the Toshiba Hardware utility is not present, try the F2 key method and the Esc key method (see below). The Toshiba Hardware utility may be downloaded from the Toshiba support website at http://support.toshiba.com

 

If the computer is fully off, and/or to avoid having to re-start it (and Windows), use one or the other of the following two methods. The PC will have to be truly off (not suspended, or in standby mode, or in hibernation mode). If an external keyboard is attached to the notebook (either directly or via a docking station or a port-replicator), disconnect it until you have completed this procedure.

 

Esc key method

Turn the computer on. If you do not see a prompt to press the F2 key, then immediately press and hold the Esc key for three seconds, and then release it. When prompted to, press the F1 key. The Setup screen will appear.

 

Toshiba desktop PCs and servers

Press and hold the F2 key immediately after turning the computer on, during the Power-on Self Test (POST).

Contributors