04-16-2012 05:46 AM
after installing win 8 consumer preview 32 bit.......i now see that my fn key is not working on my toshiba satellite c655-s5206
04-18-2012 08:45 AM
I believe that should be controlled by TVAP (Toshiba Value Added Package). Because Windows 8 isn't officially supported, there is no TVAP for Windows 8 currently. You could try downloading the one for Windows 7 to see if it will install, but I don't know if it will.
Toshiba Value Added Package(v1.6.1; 07-26-2011; 174.09M)
05-17-2012 11:04 AM
I got the FN keys to work (flashcards) by downloading toshiba value added package for windows 7 and running it in compatibility Windows 7 mode. Also, the instalation took ridiculously long (about an hour) consuming 30% cpu, but eventually it finished.
05-29-2012 02:25 PM
I keep getting "Setup TVAP error. [0x8146045B). Should I also use Win 8 as primary OS?
09-18-2012 01:44 AM
Just thought I would add that the beta VAP package for windows 8 can be downloaded at this link
Hope this helps
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.