How can I make Windows 8 seem more like Windows 7?

0
Started ‎06-01-2012 by
Modified ‎04-25-2013 by

How can I make Windows 8 seem more like Windows 7?

Question

How can I make Windows 8 seem more like Windows 7?

Answer

Windows 8 looks different than Windows 7 but still retains all functionality. However, some people may want Windows 8 to resemble Windows 7 more closely.

 

Launching the "Desktop" application from the Start screen will open Desktop mode, which looks very similar to the Windows 7 interface. However, there is no Start Menu. The Start screen is used for tasks that once were launched from the Start Menu.

 

To emulate the Start Menu:

 

  1. Right-click on the taskbar.
  2. Select "Toolbars".
  3. Select "New toolbar..."
  4. In the "Choose a folder" window, click in the address bar in the blank space to the right of the current folder to place the cursor in the address bar.
  5. Type "C:\ProgramData\Microsoft\Windows\Start Menu\" in the address bar and press ENTER.
  6. Click the "Select Folder" button. There will now be a toolbar on the taskbar titled "Start Menu" that emulates the old Start Menu. Changes to this folder will also effect the "All apps" section of the Start screen.
Comments
by KathiC on ‎01-16-2013 07:19 PM

Step 5... there is no "ProgramData" folder!

by Beecher on ‎02-19-2013 08:25 AM

Can;t find a "ProgramData" folder under the C: drive

by Administrator Administrator on ‎02-20-2013 02:26 PM

KathiC & Beecher, Windows has hidden the "ProgramData" folder by default so you won't see it when browsing the file system, but if you follow the step-by-step instructions in this article it will work as described.

 

Jim

 

Contributors