Re: my fn key is not working

Reply
Member
Posts: 1

my fn key is not working

after installing win 8 consumer preview 32 bit.......i now see that my fn key is not working on my toshiba satellite c655-s5206

Posts: 21,719
Topics: 70
Kudos: 849
Solutions: 483
Registered: ‎10-04-2011

Re: my fn key is not working

I believe that should be controlled by TVAP (Toshiba Value Added Package). Because Windows 8 isn't officially supported, there is no TVAP for Windows 8 currently. You could try downloading the one for Windows 7 to see if it will install, but I don't know if it will.

 

Toshiba Value Added Package(v1.6.1; 07-26-2011; 174.09M)

- Peter
Member
Posts: 4

Re: my fn key is not working

I got the FN keys to work (flashcards) by downloading toshiba value added package for windows 7 and running it in compatibility Windows 7 mode. Also, the instalation took ridiculously long (about an hour) consuming 30% cpu, but eventually it finished.

Regular Contributor
Posts: 152

Re: my fn key is not working

I keep getting "Setup TVAP error. [0x8146045B). Should I also use Win 8 as primary OS?

Qosmio X870-BT3G23
Highlighted
Member
Posts: 7

Re: my fn key is not working

Just thought I would add that the beta VAP package for windows 8 can be downloaded at this link

 

Hope this helps