Windows 8 and Function Keys

Reply
Member
Posts: 2

Windows 8 and Function Keys

my function keys do not function correctly after installing windows 8.   the f1 / f2 keys seem to put the computer to sleep rather than adjust brightness .   and the wifi button does not seem to turn wifi / bluetooth on / off  and  before windoes 8 i didnt have to hole the fn key down to use these buttons and now i do.  any suggestions?

Posts: 21,719
Topics: 70
Kudos: 849
Solutions: 483
Registered: ‎10-04-2011

Re: Windows 8 and Function Keys

Can you check the laptop's full model and part numbers from the label on the bottom? Don't include the serial number.

 

Did you use the Toshiba Upgrade Assistance when upgrading to Windows 8?

- Peter
Member
Posts: 2

Re: Windows 8 and Function Keys

I'm trying to find the option window to make th F1-F12 keys the primary, instead of the Fn keys (brightness, volume, etc.)

But windows 8 is being obstinate about it, and all the online help I find works only for windows 7 (using the start menu, or Run) and I'm becoming frustrated. 

I know there's an option to make the F1-F12 the primary function of those keys, but I can't find it.

Posts: 47,962
Topics: 85
Kudos: 9,136
Solutions: 3,232
Registered: ‎12-04-2008

Re: Windows 8 and Function Keys

Which computer? There is a label on the bottom.

 

How depends upon whether Windows 8 is preinstalled or not.

-Jerry
Channel 9