Toshiba C875-S7303 mouse problem with Windows 8

Reply
Member
Posts: 1

Toshiba C875-S7303 mouse problem with Windows 8

Using Windows 8 all day with my new computer and then the mouse froze.  I did the basic reboot and restarts to no avail.  When I figured out how to get to the control panel and to the mouse setting I found it had been changed to "other pointing device" not the "snaptics Touchpad V7.2" that it should be.  Easy switch, except every time I switched it back it defaults to the "other pointing device".  Any suggestions on what is wrong?

 

Tom

Posts: 47,490
Topics: 83
Kudos: 9,022
Solutions: 3,198
Registered: ‎12-04-2008

Re: Toshiba C875-S7303 mouse problem with Windows 8

[ Edited ]

 

Satellite C875-S7303

 

Downloads here.

 

 

I would try reinstalling the driver, Tom.

 

   Synaptics TouchPad Driver

-Jerry
Channel 9
Member
Posts: 2

Re: Toshiba C875-S7303 mouse problem with Windows 8

How do i reinstall driver can't get to that menu
Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba C875-S7303 mouse problem with Windows 8

sylfrmcoal, this is an old post.

What laptop do you have? Are you also having a problem with your touchpad? What menu?

- Peter