Function Keys on Windows 8.1

Reply
Member
Posts: 3

Function Keys on Windows 8.1

Hi, New to these forums so I'm not totally sure this is where this needs to be, but going to give it a shot. I am wondering if there's a way to disable or edit what the Function Keys do on Windows 8.1. I have a Toshiba Satellite Laptop, it came with Windows 8 on it and I recently updated it to Windows 8.1. I play an online game which allows you to use Function Keys to use certain things in the game, but with the way it is right now, it just controls functions on the actual laptop (such as brightness, disable/enable touchpad and pause/play a song) but I am wanting to see if I can change some of them so that I can use a couple of them on the game I play. Thank you for your help in advance!
Posts: 4,875
Topics: 57
Kudos: 1,658
Solutions: 379
Registered: ‎05-03-2009

Re: Function Keys on Windows 8.1

At the Start screen, activate the Charms Bar and click on  Settings.  Click on Change PC Settings and then click on Keyboard.  There you have a choice of how the F keys work.  The one you want is to require pressing the FN key plus an F Key to do the computer functions. That should leave the F key pressed by itself to do what you want.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 3

Re: Function Keys on Windows 8.1

 

This is what I see when I get the Charms bar up and click settings and then Change PC Settings. I don't see "Keyboard" anywhere. I see the "Keyboard" option on there but it's not lit up, it's not clickable.

 

Posts: 4,875
Topics: 57
Kudos: 1,658
Solutions: 379
Registered: ‎05-03-2009

Re: Function Keys on Windows 8.1

Your "pictures" are worthless.  I get nothing here but a big triangle! Try posting them as Attachments. However, there are two other ways to explore.  Some Windows 8 machines still have a folder called "HWSetup".  At the Start screen, type HWSetup and if you have it, look under the Keyboard tab for the setting we've been talking about.

 

If you also do not have the HWSetup folder, shutdown the computer while holding down the Shift key.  On startup, tap the F2 key until the BIOS (AKA UEFI) shows.  Look under the Advanced tab for the setting.  If not there, look around elsewhere in the BIOS.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 3

Re: Function Keys on Windows 8.1


HKM
Member
Posts: 1

Re: Function Keys on Windows 8.1

I changed my F-keys options by accident. They used to do the printed functions such as brightness and volume without the FN key, but now they require it to be pressed. My problem now is that I know what to do, but whenever I go to the Keyboard menu, there is no option to change the FN settings... Has something changed with an update, or must I enable something else first? Thank you.

Posts: 4,875
Topics: 57
Kudos: 1,658
Solutions: 379
Registered: ‎05-03-2009

Re: Function Keys on Windows 8.1

[ Edited ]

Try this HKM.  At the Start screen, type System Settings and hit Enter.  Click on Keyboard and change the setting of Function Key Mode. You gave me no info about your computer or OS.  I'm assuming you are using Windows 8.1 OEM.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit