Reply
Member
lenlen71
Posts: 1
0

invalid product key

hi all 

i have a toshiba satellite L645-S4102 window 7 i tried installing a software & it's giving me an error because it is saying that i need window7 or higher (well thats what i have) so i tried installing the microsoft office 2010 that came with it another msg came "invalid product key" so i tried the solution that the toshiba recommended to go to the start menu and then used the number 2 option ( i dont have no 2 option) i have the microsoft starter kit. so what do i do now? i have been trying  for the last 4hrs on all the solutions i read still nothing is working. Please help!!

Regular Contributor
LaptopDan757
Posts: 70
0

Re: invalid product key

The MS Office 2010 that ships with most laptops is a Trial version that allows you up to 25 total launches. You must purchase a MS Office Product Key that matches the software application installed in order for it to activate properly.

i.e., if you have the MS Office 2010 Pro edition installed then you must purchase a Pro liscense to get the proper 25 didgit key code. If you have the Home and business version then you must purchase a H&B liscence...etc.

"My comments are my own reality" Consider these in addition to other sources. I only know what I know.
Dan
Ace Advisor
Jerry_Lippey
Posts: 33,108

Re: invalid product key

[ Edited ]

 

Satellite L645-S4102

 

 

Following is from the fine print in the spec above.


Microsoft Office Starter 2010. Office Starter consists of reduced-functionality versions of Word and Excel with advertising. PowerPoint, Outlook, OneNote, Access and Publisher are not included.

 

Includes Microsoft Office 2010 preloaded. Purchase a Product Key to activate a full Microsoft Office 2010 suite.


So you can use Starter with no strings. In order to use the real Office 2010, you must purchase a product key.

 

   Microsoft Office 2010 Starter Edition Functionality

 

   Office Product Key Card frequently asked questions

 

In case that's not sufficient: We can't see what you're doing. You'll need to explain in far more detail. And any error message you provide is useless unless you quote it exactly on a line by itself. Otherwise, we cannot look it up.

-Jerry
Super Advisor
brad
Posts: 1,052
0

Re: invalid product key

In addition to the advice already given...

 

Where are you getting the Product key that you are entering?  It isn't the one from the bottom of the computer that you need.  I believe that for the Office products there is a card in the documentation someplace with the correct key on it, it's basically just a post card size piece of heavy paper with the product key hologram sticker on it.