Windows 7 upgrade install issue

Reply
Member
Posts: 3

Windows 7 upgrade install issue

HI, I am looking for help for my Realtek wireless lan......

I have purchased back in October a:

Toshiba Satellite P505d-S8930

Serial #89025824W

Part # PSPFOU-005003

 

I Received the windows 7 upgrade DVD from Toshiba and installed the windows 7 to my computer...The problem I  have is the Realtek wireless lan is now not working. It tells me to reinstall the driver but when I do that the system tells me the newest version is already installed. When I try to connect from the "network and Sharing Center" it is not an option. I have to go back to using the Ethernet cable to get the internet.....Can anyone help? I really would like to use the wireless.

 

Any help would be greatly appreciated, Thanks.

Occasional Advisor
Posts: 300

Re: Windows 7 upgrade install issue

the windows vista driver will work , need to locate tosapins folder either in c:\ or c:\programsfiles\toshiba

but if you did clean install download driver from toshiba website 

edw
Member
Posts: 1

Re: Windows 7 upgrade install issue

Have similar problem with Realtek driver.  Did 'clean install' of Win 7.  Then to Realtek and downloaded new driver.

Unable to install driver so did a restart.  Taskbar showed 'installing driver'  then got blue screen advising sys would shut down due to impending crash.  Then started in safemode w/networking, downloaded driver again, attempted

run 'setup' but received message "sorry we do not support this operations system."  Thought I would just clean all off and start from scratch, but it will not let me reformat either.

 

Member
Posts: 3

Re: Windows 7 upgrade install issue

Thanks for the response......I did the install from the Toshiba web site but it still didn't work. Any other suggestions?

Member
Posts: 6

Re: Windows 7 upgrade install issue

One Question, did you uninstall the driver before upgrading? This may be the problem. The old one is stuck.
Member
Posts: 3

Re: Windows 7 upgrade install issue

yep...I uninstalled the realtek driver but not until after I installed the windows 7. Do you think that would make a difference? The download instructions didn't say to uninstall drivers.....I'm wondering if I should run the back up discs to get the laptop to the original format and start again? What do you think?