After a Windows 7 update last week my laptop can't run with the NVIDIA drivers. I tried the ones from the Toshiba website and from NVIDIA and the default ones that Windows Update wants to install. All of them cause the machine to crash and not be able to startup. I ended up installing a fresh copy of Windows 7 and can reproduce the issue. Are there any drivers for the NVIDIA Quadro NVS 130M that will work with the latest Windows updates? Has anyone else seen this issue? My computer was running great for years until this issue popped up last week. I'm not sure which update causes the problem unfortunately.