Reply
Member
Posts: 1

Startup Freeze in Windows 7?

Have the same problem with Vista and Windows Server 2008. I'm using Satellite P205-S6307, lately I upgraded to Windows 7 RC1, when I shutdowned in the normal way, next time I powered on my laptop and logged on to windows and it just freezed at welcome screen, or sometimes it passed the welcome screen but the desktop had nothing but black background with mouse and the line "Windows 7 Evaluation copy, Build 7100". If I hold the power button for 5s to shutdown the laptop and then power on, when the welcome screen appears I press shutdown and then power it on again, this time I can log onto windows.

 

I downloaded the hotfix for Vista but cuz it had the extension .msu, I couldn't force it run with compatibity mode. Can anyone help me with this? Thanks a lot in advance!

Serge Wazuki