Blue Screen - Driver Power State Failure

Reply
Member
Posts: 5

Blue Screen - Driver Power State Failure

My laptop does not shut down completely when powered off. I got a blue screen indicating that there was a Driver Power State Failure. I got someone to review the dump files from the last two failures. There seems to be an issue with my iastor driver (Version 8.9.2.1002). I've been trying to find an update to the drive, but can't find one in the support section on the site. Can someone help me out here? 

 

P.S. My BIOS is INSYDE 1.70 , 09/15/2009; model number A500-ST5601; Part number PSAP0U-00S007

Frequent Advisor
Posts: 2,022

Re: Blue Screen - Driver Power State Failure

[ Edited ]

check this out. there are links to other threads that may be helpful. communities.intel.com/message/71147;jsessionid=D8896983A42EC2B54B50DF0DBB47B6B8.node5COMS

-civicman4-
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Post all info about your laptop and version of windows. We are working on it but still do not have the powers to read your mind.
Posts: 47,945
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Blue Screen - Driver Power State Failure

 

Satellite A500-ST5601

 

Bug Check 0x9F: DRIVER_POWER_STATE_FAILURE 

 

Have you installed Service Pack 2?

 

Please attach a relevant mini-dump file to your reply.

-Jerry
Channel 9
Member
Posts: 5

Re: Blue Screen - Driver Power State Failure

I'm not sure that I've installed service pack 2. Will check later today. I can't seem to get the dump uploaded onto this forum. Please download file from the first post in this discussion forum: http://www.sevenforums.com/crashes-debugging/83554-blue-screen-driver-power-state-failure.html

Posts: 47,945
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Blue Screen - Driver Power State Failure

[ Edited ]

There seems to be an issue with my iastor driver (Version 8.9.2.1002).

I don't know why the disk driver is implicated. The results of the two mini-dump files from BlueScreenView are below. Those from Dumpchk.exe are attached.

 

It wouldn't hurt to try replacing the sound driver.

 

   Realtek Audio Driver for Windows Vista (32bit/64bit)

 

==================================================
Dump File         : 050810-27908-01.dmp
Crash Time        : 5/8/2010 10:11:04 AM
Bug Check String  : DRIVER_POWER_STATE_FAILURE
Bug Check Code    : 0x1000009f
Parameter 1       : 00000000`00000004
Parameter 2       : 00000000`00000258
Parameter 3       : fffffa80`03ce4680
Parameter 4       : fffff800`00b9c4d0
Caused By Driver  : Wdf01000.sys
Caused By Address : Wdf01000.sys+39800
File Description  :
Product Name      :
Company           :
File Version      :
Processor         : x64
Computer Name     :
Full Path         : C:\test\050810-27908-01.dmp
Processors Count  : 2
Major Version     : 15
Minor Version     : 7600
==================================================

==================================================
Dump File         : 050610-23727-01.dmp
Crash Time        : 5/6/2010 12:10:28 PM
Bug Check String  : DRIVER_POWER_STATE_FAILURE
Bug Check Code    : 0x1000009f
Parameter 1       : 00000000`00000004
Parameter 2       : 00000000`00000258
Parameter 3       : fffffa80`03d00040
Parameter 4       : fffff800`00b9c4d0
Caused By Driver  : ntoskrnl.exe
Caused By Address : ntoskrnl.exe+764da
File Description  :
Product Name      :
Company           :
File Version      :
Processor         : x64
Computer Name     :
Full Path         : C:\test\050610-23727-01.dmp
Processors Count  : 2
Major Version     : 15
Minor Version     : 7600
==================================================

-Jerry
Channel 9
Member
Posts: 5

Re: Blue Screen - Driver Power State Failure

-I'm running Win 7 and all Microsoft updates are installed. Thinking about reverting to version 8.8 of the iaStor driver,  but I'll need to back up my files first. 

Posts: 47,945
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Blue Screen - Driver Power State Failure


-I'm running Win 7.. 


Why didn't you say so?!

 

That machine comes with 64-bit Vista.

-Jerry
Channel 9
Member
Posts: 5

Re: Blue Screen - Driver Power State Failure

It came with Vista-64 and I upgraded to Win 7. Should I use the drivers that come with that version instead of using the relevant Windows 7 ones?

Posts: 47,945
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: Blue Screen - Driver Power State Failure


Should I use the drivers that come with that version instead of using the relevant Windows 7 ones?

Use Windows 7 drivers.

-Jerry
Channel 9