How To: Upgrading from Windows Vista to Windows 7

0 Kudos
Started ‎06-12-2012 by
Modified ‎06-12-2012 by
(6,684 Views)

Depending on your hardware and your current edition of Windows Vista, you can use the Upgrade option during Windows 7 installation to upgrade from Windows Vista to a corresponding or higher edition of Windows 7. For more information, see Windows 7 system requirements.

 

Upgrading is the most convenient way to get Windows 7 on your computer, because it keeps your files, settings, and programs from Windows Vista in place.

 

If your current edition of Windows Vista can't be upgraded to the edition of Windows 7 that you want to use, you can still install Windows 7 by using the Custom installation option instead. However, the Custom option doesn't preserve your files, programs, or settings.

Click here for instructions on upgrading from Vista to Windows 7

 

For a step-by-step tutorial on how to perform a custom installation, see Upgrading from Windows Vista to Windows 7 (custom installation).

 

The TOSHIBA WINDOWS 7 Support Page will answer TOSHIBA laptop specific questions and can be accessed by CLICKING HERE.

Contributors