DR430 Error Message Program cannot be recorded in video mode E27

Reply
Member
Posts: 1

DR430 Error Message Program cannot be recorded in video mode E27

Any help to correct this error message and record on DVD-R media would be appreciated.

 

 

Occasional Contributor
Posts: 10

Re: DR430 Error Message Program cannot be recorded in video mode E27

Hello

 

Am getting same message. When I attempted to do what the book indicated which is to format the disc to record as VR mode, I was unable to then format the disc to be VR mode as the format disc mode was grayed out once a blank disc was put in and would not automatically format disc when a blank disc was loaded even though I had indicated in Setup that the disc format mode should be VR.  Have not been able to get an answer from technicians or anyone to resolve this. Am tempted to return before 15 days and purchasing from another manufacturer.

Member
Posts: 2

Re: DR430 Error Message Program cannot be recorded in video mode E27

Hello- 

I have a DR430 and  Will not record just out "out of the Blue"- same DVD's ive been using for almost a year- still under warr- i can record some stuff then get error E27- just the one program i have rocorded on my PVR- but i can record anything from the same channel that was recorde same day within hours of same program?? Unbelievable i was up until 4am last night - couldnt figure it out!!

Member
Posts: 2

Re: DR430 Error Message Program cannot be recorded in video mode E27

also unable to change format dvd-r disc- dvd format is "greyed out"