07-29-2010 10:29 PM
Solved! Go to Solution.
07-31-2010 12:35 PM
Sounds like your display settings on your laptop got changed. When you say "serial" cable from your laptop to your TV - do you mean VGA to VGA cable from computer to TV? Your TV manual/specs will tell you what native resolutions each input accepts (1024x768, etc) - you need to set your vid card settings/refresh rate to that resolution/refresh rate to correctly display the image on your TV.
Nate
07-31-2010 12:59 PM
Thanks Nate. Yes, I do mean the svga cable. My husband brought his laptop from work so we could try it and his works fine so I set all the settings (refresh rate and resolution) to match his and it still won't work. Now I'm totally confused! Any other suggestions? :/
07-31-2010 01:18 PM
What is the model number of his laptop? Satellite Pxxx-xxxx., etc - on a sticker on the bottom of the laptop.
Nate
07-31-2010 07:47 PM
07-31-2010 08:48 PM - edited 07-31-2010 08:49 PM
Read pages 68-70 - the .pdf is locked and will not let me copy/paste ![]()
Nate
07-31-2010 09:46 PM
08-01-2010 07:10 AM
Did you get the part about using the FN key along with the F5 to shift between the different display configurations that the Toshiba offers? You may not be sending a signal to the TV at all with the Toshiba and you have to activate it through the FN + F5 key strokes. Also... set the Toshiba to the res you set the Dell to.
Nate
08-01-2010 06:39 PM
I already knew about the Fn+F5 key. I used it all the time back when it did work to switch from sending the signal to TV to sending it only to the notebook. I set all the settings on the Toshiba to match the settings on the Dell and that also didn't work. I looked up what settings are supported by the Toshiba Regza TV manual as well ( that is the TV I am trying to hook it up to again) and none of the settings it says it accepts worked. There must be some kind of problem with the signal my laptop is sending out now. I'm trying to figure out at this point whether it is a driver problem or a hardware problem. In either case I KNOW it's a problem with the laptop and not the cable or the TV.
08-04-2010 08:36 PM
Well, I reformatted my hard drive and restored my laptop and that still didn't fix it. This confirms it is a hardware issue with the port and since it is one piece with the motherboard the entire motherboard would have to be replaced if they couldn't fix it by hand. Cheaper to but a new laptop! The work around solution is to buy a usb to vga conversion cable. I'm told it will work just as well. Good luck to all of you who are having the same problem.
08-06-2012 06:24 PM
I want to connect my pc to my Toshiba 46SL412U television, but every time I do so (with my vga cord, or maybe it's s-vga, don't know the difference), it tells my "unsupported video signal". I have a ATI Radeon HD 3600 video card. Can my card show video on the TV? If so, what do I need to do?
Any help would be very appreciated!
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.