Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

Reply
Member
Posts: 3

Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

Yeah.... The title is what i'm trying to setup. Problem is the tv never flickers/shows any signs of connection, other than the laptop's display (resolution menu) lists the monitor as a viziohdtv.... but beyond that it never connects. I've try all the fn stuff, i've tried clone/extended. I've restarted with it plugged in/turned off so on and so forth.

What I've detirmened the problem to be is a driver one. So I go to the toshiba website and look up the model and I find...... Nothing for model "c655-s5512" So... whatsup?

Can I get a hook up with some drivers or something? Cause I'd really like to get it hooked up for my dad.\

 

Thanks.

Member
Posts: 3

Re: Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

Only have a few days until i'll be out of town and not be able to help him so.... if i could get some help on some possible drivers I don't seem to be able to find on the site (model c655-s5512) not listed. Whatevers clever

Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

Can you tell me the notebook's model-part number? It should be on the label on the bottom along with the model number, and it should start with a 'P'.

 

Try one of these.

 

Intel Display Driver(v8.15.10.2353; 04-08-2011; 82.2M)

nVidia Display Driver(v8.17.12.6744; 03-08-2011; 160.82M)

 

Before you install them, you might want to create a System Restore point because I'm not sure of your model.

- Peter
Posts: 46,745
Topics: 83
Kudos: 8,776
Solutions: 3,144
Registered: ‎12-04-2008

Re: Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

[ Edited ]

 

Satellite C655-S5512 (PSC2EU-04U047)

 

Walmart spec above.

 

Satellite C655-S5512 (PSC2EU-00R00F) 

 

Drivers are here.

-Jerry
Channel 9
Member
Posts: 3

Re: Windows 7 Vga Vizio tv connection with Toshiba Satellite c655-s5512

Thank you very much for the info, I'll give a go next time i'm over. Hopefully it is just a driver problem and I can get it going.

 

Thanks ^_^