Toshiba webcam crashes flash plugin

Posts: 2

Toshiba webcam crashes flash plugin



I have a Toshiba Satellite L650-116

Part number PSKIJ 00800EG3

running Windows 7 (64-bit)

everything works fine until I try to use my webcam to broadcast live video streams using a browser.

This causes The flash plugin to crash in IE9, firefox 13 and Google chrome.

Also I installed manycam and this program Also does not detect my webcam which is listed as "Toshiba webcam" under device manager.

The webcam does work however but only if I use web camera application or yahoo messenger.


This is not related to the flash version. The problem appears with the latest flash player versions and previous ones.

This problem is also discussed on The adobe forums here


any suggestions?


All Replies
Posts: 2

Re: Toshiba webcam crashes flash plugin

I can now tell that this is a Toshiba problem! same computer, same configuration but a different webcam and the flash plugin is working as it should!