02-15-2011 11:36 AM - edited 02-15-2011 11:55 AM
I have a toshiba satellite l305-s5885 it had windows vista on it the vga card is 128 MB , i install a windows 7 on the laptop it says that the vga card is 64 MB and the games make a warning that my vga card is 64 , even i downloaded the driver from toshiba.com what can i do.
thx
02-15-2011 12:39 PM
Try installing the chipset driver for that model.
http://cdgenp01.csd.toshiba.com/content/support/do
02-15-2011 03:52 PM
sorry it still not working
thank u for ur effort
02-16-2011 10:40 AM
Have you tried installing the driver for your graphics card?
02-18-2011 07:04 AM
yes i installed it and nothing new.
02-24-2011 08:54 AM - edited 02-24-2011 09:02 AM
Thats a tough one. Try installing the newest video driver for it from intel.
Are you using the original ram in it or have you upgraded?
The graphics use dynamically allocated ram. That means system ram is used for the graphics and it is just possible that 64 is all that it has available for graphics under windows 7.
It may help to increase the system ram up to it's max of 4 gigs. Your system came with 3 gigs of ram, 2 gig and 1 gig sticks.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.