The Intel HD Graphics 3000 (XP Pro x64 SP2) drivers didn’t work with my Toshiba Satellite L755-S5107

Reply
Member
Posts: 2

The Intel HD Graphics 3000 (XP Pro x64 SP2) drivers didn’t work with my Toshiba Satellite L755-S5107

[ Edited ]

Hi Everybody;

I downgrade my OS to Windows XP Professional x64 b; and i have a big problem to find a graphic driver; as i tried all Intel HD Graphics XP Pro 64bit drivers available in Intel download server.

Please can you help me to fix this problem? My Laptop specifications are below:

Toshiba satellite L755-S5107, S/N: XXXXXXXXX, Model: Intel_Mobile

 

BIOS INSYDE V3.10, Board Product ID: Base Board Product Name

 

Processor Information

Summary: 1 Physical Processors / 2 Cores / 4 Logical Processors / 64 bits

Name: Intel(R) Core(TM) i3-2350M CPU @ 2.30GHz

Vendor: GenuineIntel

Original System Clock: 100 MHz

Display Adapter Information

Intel(R) HD Graphics Family 1797 MBytes

Sound Adapter Information

Conexant SmartAudio HD Conexant

Intel(R) Display Audio Intel(R) Corporation

Operating system:

Windows XP Professional (x64)

 

Thanks a lot and I appreciate your help.

 

Regards

Nadir

 

 

 

[Moderator edit to remove serial number.]

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: The Intel HD Graphics 3000 (XP Pro x64 SP2) drivers didn’t work with my Toshiba Satellite L755-S

XP display drivers were not released for that model. That model was released with Windows 7.

- Peter