TV Ouput for Toshiba Satellite A305-S6905

Reply
Member
Posts: 2

TV Ouput for Toshiba Satellite A305-S6905

Does Toshiba Satellite A305-S6905 have any output so that I can connect this laptop to my tv when watching movies? I have a Samsung HDTV. I also have got  1.5m VGA SVGA HD15 M-M Male Lead Cable LCD Monitor and VGA to 3 RCA Component Cable For PC RGB HD TV LCD. Can these work? If yes, then how?

Posts: 47,512
Topics: 84
Kudos: 9,030
Solutions: 3,200
Registered: ‎12-04-2008

Re: TV Ouput for Toshiba Satellite A305-S6905

 

Satellite A305-S6905 

 

See the specs above. There's only an RGB/VGA (monitor) port for video output (at the rear on the left side). You'll need to get audio from the headphone jack on the front.

 

Since you don't tell us the model of the Samsung TV, there's no way to look up its inputs. This one, for example, has the monitor input.

-Jerry
Channel 9
Super Advisor
Posts: 1,052

Re: TV Ouput for Toshiba Satellite A305-S6905

Just a note on those VGA to Component cables:  They are not for connecting  a VGA signal to Component connectors, the signals are not compatible.  If all you have are Component connections on your TV, then you need a VGA to Component Converter box.  Quality and price apparenty vary greatly on the converters.

Member
Posts: 2

Re: TV Ouput for Toshiba Satellite A305-S6905

the model of the samsung TV is LN40A530P1FXZA.

 

I tried connecting the VGA Cable but nothing happened.

 

thanks for the advice anyways Smiley Happy

Posts: 47,512
Topics: 84
Kudos: 9,030
Solutions: 3,200
Registered: ‎12-04-2008

Re: TV Ouput for Toshiba Satellite A305-S6905

According to the User's Manual for your model, you need a conversion cable to, for example, S-Video.

 

This cheapie would do.

-Jerry
Channel 9