Reply
Member
Posts: 1

Green Screen crash while streaming

Hello,

I recently purchased a qosmio x505-q898 , and I keep getting randomly a green screen eachtime I stream anything online, and the sound runs normally in the background.

To define the problem more , I get a crash the whole screen turns black then it recovers but the video goes green!! and I get a notification that the system has successfully recovered from a problem .

I am wondering if there is something I can do to fix this or is this a hardware problem?

 

Many thanks,

 

 

Super Advisor
Posts: 4,069

Re: Green Screen crash while streaming

I'm not sure if this is your problem or not, but it sounds like it might be.  So, give this a try first.

 

There is a known bug in Flash Player, which will cause a YouTube display to turn black when full screen. Adjusting the following Flash Player setting should fix it.

 

While the video is playing, right-click on it and click Settings. Uncheck the box for Enable hardware acceleration.

 

Mike