Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

Reply
Member
Posts: 7
Accepted Solution

Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

Running a Qosmio Q305 Q706.  I have an external monitor attached and it shows on the NVIDIA control panel.  Here's the problem.   I can switch between one (Laptop LCD) or the other (External LCD) but CANNOT get the dual mode to show where I can mirror or extend my desktop.

 

I have uninstalled the video drivers and reinstalled.

 

Tried to boot and then attached the external LCD screen

 

Attached and booted

 

I got it to work once (not sure why) and the next time i powered up back to the same problem.  No errors in the device mamanger. 

 

I contacted Toshoba support and was raised to a higher level problem so the support rep had to pass off to a supv.  Was told they would call me right back.  Never heard back from Toshiba.

 

Any ideas!!!

 

Thanks

Member
Posts: 7

Re: Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

I solved the problem!!!!!  It was the power settings...so strange.  The NVIDIA chipset was closing off the dualview under the AC/Battery power settings.  Had nothing to do with the display drivers.

 

 

View solution in original post


All Replies
Posts: 45,983
Topics: 81
Kudos: 8,268
Solutions: 3,090
Registered: ‎12-04-2008

Re: Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

Qosmio X305-Q706 

 

Maybe this Vista stuff from Microsoft helps.

 

   Set up multiple monitors

-Jerry
Channel 9
Member
Posts: 7

Re: Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

I solved the problem!!!!!  It was the power settings...so strange.  The NVIDIA chipset was closing off the dualview under the AC/Battery power settings.  Had nothing to do with the display drivers.

 

 

Posts: 45,983
Topics: 81
Kudos: 8,268
Solutions: 3,090
Registered: ‎12-04-2008

Re: Dual monitors, cannot get the dualview or extend desktop to show, FN-F5 shows external monitor

Glad you got it solved. Thanks for letting us know the situation.


The NVIDIA chipset was closing off the dualview under the AC/Battery power settings.  Had nothing to do with the display drivers.

Strange indeed. I wouldn't have thought to look there.

 

Mind sharing what detective work led you to that discovery?

-Jerry
Channel 9