Does anyone know why my built in webcam is not connected?

Reply
Member
Posts: 5
Accepted Solution

Does anyone know why my built in webcam is not connected?

I have the built in webcam on my laptop and it keeps saying "no webcam found check to see if your web cam is connected" every time I turn the camera on. I think I might have turned off something or worse, removed it by mistake.. I just got the laptop 4 days ago and it took me a while but I got it to work the first day so I know its not broken. Im pretty sure I did something when I was messing with the control panel. Is there a way I can reinstall it?


Accepted Solutions
Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

Yes, that was it!

 

First, try reinstalling the webcam software.

 

Toshiba Web Camera Application(v2.0.3.3; 06-02-2011; 86.42M)

 

If that doesn't work, we could try a restore. Has it worked recently? If it has, or if you're not sure, try using System Restore to restore a previous restore point from before this became an issue. Note that this will not alter your personal data.

 

If the System Restore doesn't help, we could check if another application is interfering. If you have any video conferencing software installed such as Skype, try uninstalling it and then reinstalling the "Toshiba Web Camera Application" I linked above. If it works, you could then reinstall Skype.

- Peter

View solution in original post


All Replies
Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

What model is your notebook? It should be listed on a label on the bottom.

- Peter
Member
Posts: 5

Re: Does anyone know why my built in webcam is not connected?

the system unit is  c655d s5330. is that the number you are asking for?

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

Yes, that was it!

 

First, try reinstalling the webcam software.

 

Toshiba Web Camera Application(v2.0.3.3; 06-02-2011; 86.42M)

 

If that doesn't work, we could try a restore. Has it worked recently? If it has, or if you're not sure, try using System Restore to restore a previous restore point from before this became an issue. Note that this will not alter your personal data.

 

If the System Restore doesn't help, we could check if another application is interfering. If you have any video conferencing software installed such as Skype, try uninstalling it and then reinstalling the "Toshiba Web Camera Application" I linked above. If it works, you could then reinstall Skype.

- Peter
Member
Posts: 5

Re: Does anyone know why my built in webcam is not connected?

its connected now, I cant believe I uninstalled it by accident. thank you 1 million times!!

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

No problem at all! Thanks for letting us know what fixed it for you. If something's acting up, reinstalling the software/driver is often an easy solution!

- Peter
Member
Posts: 2

Re: Does anyone know why my built in webcam is not connected?

My webcam is doing the same. It will have the blue light on, but you cant see anything. My side is black. I have tried to uninstal it, and reinstal it. and it still isnt working. i had skype downloaded, but i uninstaled that and reinstaled the webcam and still nothing. i have even tried the system recover. it still only shows the blue light, but no picture! its very aggrevaiting!!

 

-Brittany

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

Brittany, have you double-checked that there isn't a protective film on the camera? It can sometimes be easy to miss. I believe some models have two - one that's wide and covers the entire area and another small one that covers just the camera. Not all have this, but some do. Ensure that there's no film on it. If there isn't, and you've alraedy performed a full system recovery, it sounds like your machine needs servicing.

- Peter
Member
Posts: 2

Re: Does anyone know why my built in webcam is not connected?

My laptop seems to be weirder. It shows the webcam chicony under imaging devices with a yellow icon under it. And no application can detect the webcam. Tried the webcam application u listed before but even that does not detect the webcam! Smiley Frustrated What to do?

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

shahabusmani, try right-clicking it in the Device Manager and uninstalling it. Then redownload the web cam application and install it.

- Peter
Member
Posts: 1

Re: Does anyone know why my built in webcam is not connected?

[ Edited ]

Hey whenever i log in to my laptop it say web cam application initialization failed. Ive tried downloading a web cam application but i still cant get it to work 

btw i have a toshiba satellite - a665-s5170

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

Try looking at this article.

 

How can I fix my webcam?

- Peter
Member
Posts: 1

Re: Does anyone know why my built in webcam is not connected?

Hello,

I am having trouble getting to my webcam as well.

Originally I had the tool bar for the webcamera on a tab on my desktop. It got quite annoying so I closed it.

Ever since then I have been unable to find my webcam when searching my computer under any libraries. In addition I cannot find a driver to re- install it with on the toshiba website. I would appreciate some help if you have the time.

My model is the X505-Q8102.

 

Thanks -Gas

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Does anyone know why my built in webcam is not connected?

Is your model the X505-Q8102X?

 

This is the latest version of your webcam software.

 

Toshiba Web Camera Application(vV2.0.3.37; 05-30-2012; 86.43M)

 

You should be able to type "camera" into the Start Menu's search field to find it.

- Peter
Member
Posts: 1

Re: Does anyone know why my built in webcam is not connected?

I'm having the same problem and by reading this, I believe I have accidently uninstalled my Webcam Application too but I don't know where to reinstall it. Under device manager it says my webcam is up to date and I've used it before but it seems as it disapeared! I can use my webcam if I have another app working it such as Skype or Pixtect.com but I cannot use it just for webcam just by itself or on Facebook. I have a Toshiba Satellite C655-S5512. Thanks.

Posts: 4,934
Topics: 57
Kudos: 1,734
Solutions: 389
Registered: ‎05-03-2009

Re: Does anyone know why my built in webcam is not connected?

[ Edited ]

HERE is the WebCamera Application for your machine if you want to try reinstalling it.

 

 

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 1

Re: Does anyone know why my built in webcam is not connected?

I think my webcam may be uninstalled because it says i dont have one and mine is built in... my laptop is a toshiba Satellite M645- S4070

Posts: 4,934
Topics: 57
Kudos: 1,734
Solutions: 389
Registered: ‎05-03-2009

Re: Does anyone know why my built in webcam is not connected?

[ Edited ]

The Web Camera Driver for your machine, Missy, is HERE. Download it and reinstall.

 

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 1

Re: Does anyone know why my built in webcam is not connected?

I have a Toshiba Satellite L855D-S5117 with windows 8.  my webcam was working fine then all of a sudden when I click on the webcam option it says "connect a camera."  the blue light on the webcam lens doesn't come on like it had previously either.  I've tried downloading a webcam application and that doesn't seem to do anything either.  I would greatly appreciate any help anyone can give me