Display driver does'nt complete setup on win 7

Reply
Member
Posts: 6

Display driver does'nt complete setup on win 7

Dear everybody , pleas I need help on this matter

 

I recently upgrade to win 7 (custom installation) and downloaded the display driver from downloads (

AMD/ATI Display Driver for Windows 7 (32/64)(v8.634.1; 09-04-2009; 113.08M) and after extracting the setup dont run ,the icon of the setup appear in the taskbar for a moment and disappear directly and setup dont run
 
I have Tosiba sattelite p305D S 8900
Posts: 47,632
Topics: 84
Kudos: 9,081
Solutions: 3,209
Registered: ‎12-04-2008

Re: Display driver does'nt complete setup on win 7

 

Satellite P305D-S8900 

 

This driver?

 

   AMD/ATI Display Driver for Windows 7 (32/64)

 

Try installing a different way. Are you able to decompress the download file and note the folder containing *.inf files (one or more)?

 

If so, come back here for more.

-Jerry
Channel 9
Regular Member
Posts: 4

Re: Display driver does'nt complete setup on win 7

[ Edited ]

I have an a305d-s6831 and I am unable to install this display driver for windows 7. The install starts but does not finish. I found the folder with the inf files. What do I do now.

Posts: 47,632
Topics: 84
Kudos: 9,081
Solutions: 3,209
Registered: ‎12-04-2008

Re: Display driver does'nt complete setup on win 7

 

Satellite A305D-S6831  

 


driver_video_amd_TC50034700F.exe

 Looks like there are two drivers listed. Have you tried them both?

 

   AMD/ATI Display Driver for Windows 7 (32/64) (Version 8.634.1 - Released 09/03/09)

   driver_video_amd_TC50034700F.exe

 

   AMD/ATI Display Driver for Windows 7 (32/64) (Version 8.593.100.5 - Released 09/03/09)

   driver_video_amd_TC50034500B.exe

 

 

Try it this way. Open Device Manager (devmgmt.msc) and expand Display adapters. Right-click the adapter, click Update Driver Software, and browse to the folder with the .inf files.

-Jerry
Channel 9
Regular Member
Posts: 4

Re: Display driver does'nt complete setup on win 7

I was able to download Version 8.593.100.5 and it installed properly. This driver for Windows 7 was not listed for my computer. Apparently the driver listed is not for my computer. Thank you very much.

Posts: 47,632
Topics: 84
Kudos: 9,081
Solutions: 3,209
Registered: ‎12-04-2008

Re: Display driver does'nt complete setup on win 7


Version 8.593.100.5  ... This driver for Windows 7 was not listed for my computer.

If you go here, you'll see your model listed.


Qosmio F40-ST4101, F45-AV412, F45-AV410, F45-AV411, F45-AV411B, F45-AV425, F45-AV423, F45-AV413
Satellite A210-ST1616, A215-S7407, A215-S7408, A215-S7414, A215-S7422, A215-S7427, A215-S7428, A215-S7433, A215-S7437, A215-S7444, A215-S7447, A215-S7462, A215-S5857, A215-S5850, A215-S5849, A215-S5825, A215-S5824, A215-S6814, A215-S6804, A215-S5822, A215-S5818, A215-S5817, A215-S5815, A215-S5808, A215-S5807, A215-S5802, A215-S7425, A215-SP5816, A215-S7417, A215-S7413, A215-S7411, A215-S7416, A305D-S6831, A305D-S6835, A305D-S6848, A305D-S6867, A305D-S6991E, A305D-S68651, A305D-S6865, A305D-SP6801, L355D-S7809, L355D-S7810, L355D-S7832, L355D-S7813, L355D-S7825
Satellite Pro A210-EZ2201, A210-EZ2202X, A210-EZ2203X
Other Models All models having model/part numbers beginning in PSAH4U
-Jerry
Channel 9
Regular Member
Posts: 4

Re: Display driver does'nt complete setup on win 7

I didn't see the driver listed here . The one(8.634.1) that doesn't work for my computer is listed though.

Posts: 47,632
Topics: 84
Kudos: 9,081
Solutions: 3,209
Registered: ‎12-04-2008

Re: Display driver does'nt complete setup on win 7

When you click on the plus sign to the left of the driver you found, the sedond one appears.

 

-Jerry
Channel 9