Chicony webcam not recongized? (GRAPH RENDER FAIL)

Reply
Member
Posts: 6

Chicony webcam not recongized? (GRAPH RENDER FAIL)

[ Edited ]

I am using the Skype and the webcam suddenly errors with "Unknown error"

I checked with Chicony Camera Asisst Software and it says "Graph Render Fail"

Any suggestions?

 

P.S. Laptop is Satellite L300 (unsure what model)

Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Chicony webcam not recongized? (GRAPH RENDER FAIL)


Satellite L300 (unsure what model)

There is a label on the bottom. What is the part number?

 

What is the service-pack level of your Windows Vista?

-Jerry
Channel 9
Member
Posts: 6

Re: Chicony webcam not recongized? (GRAPH RENDER FAIL)

PSLB0E in a SP1 Vista

Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Chicony webcam not recongized? (GRAPH RENDER FAIL)

All your drivers are here. Bookmark that URL.

 

If you have 32-bit Windows Vista, try reinstalling this camera driver.

 

   Chicony Webcam driver for Windows Vista 32 Bit, 1.7.175.0123, 04/06/08

 

   webcam-20080416144205.zip

-Jerry
Channel 9
Member
Posts: 6

Re: Chicony webcam not recongized? (GRAPH RENDER FAIL)

[ Edited ]

I has tried to download it and install it, but still errors.

Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: Chicony webcam not recongized? (GRAPH RENDER FAIL)


I has tried to download it and install it, but still errors.


Did you succeed installing it? No errors?

 

If so, try removing the driver first. Open Device Manager (devmgmt.msc), expand Imaging devices, right-click the Chicony device, and click Uninstall. Then reboot and reinstall.

 

 

Which version of Windows Vista do you have? What is the service-pack level?

 

Do you keep Windows up-to-date using Windows Update? There are reports that this helps the webcam situation.

-Jerry
Channel 9
Member
Posts: 1

Re: Chicony webcam not recognized? (GRAPH RENDER FAIL)

I have the same problem, my Chicony webcam doesn't appear at device manager....I think my lap doesn't know that have a webcam! I tried EVERYTHING! And looked EVERYWHERE!..Also a did the "recovery operation" twice  like the out box and the problem still...When I try to start the webcam appear something like this:" webcam driver open failed. Please restart camera or computer"...It always appear! Even though I reboot my lap!

 

What Can I do???

Thanks in advance.....

Member
Posts: 9

Re: Chicony webcam not recognized? (GRAPH RENDER FAIL)

Have you tried moving lid toward closed position and seeing if camera goes on?  There is a manufacturing defect with the cable between the lid and the motherboard.  It is not a software or driver problem.