Can't control screen brightness on Toshiba l650-11f

Reply
Member
Posts: 2

Can't control screen brightness on Toshiba l650-11f

Hello

I have a problem with screen brightness in Toshiba l650-11f running windows 7

 

I can't adjust screen brightness either from FN key or battery power control and it always on high brightness .

 

I try to reinstall graphic card driver and FN hot-keys driver but the problem is still here.

 

Even I reinstall the windows from the backup the problem gone for a while after that it comes again.

 

My graphic card in ATI 5650. 

Member
Posts: 2

Re: Can't control screen brightness on Toshiba l650-11f

Any help please because I can't use the laptop at night the screen brightness is too high and its hurt my eyes and I can't lower it.

Posts: 47,473
Topics: 83
Kudos: 9,018
Solutions: 3,196
Registered: ‎12-04-2008

Re: Can't control screen brightness on Toshiba l650-11f

 

Satellite L650-11F 

 


I reinstall the windows from the backup the problem gone for a while after that it comes again.

Perhaps you have installed something that makes a difference. I would restore it again and check after each installation.

 

If the problem persists after you restore the hard disk to its original out-of-the-box contents using Toshiba recovery media and before you install anything, then it can't be fixed by software. In that case, it's due to a hardware or BIOS malfunction.

-Jerry
Channel 9
Member
Posts: 3

Re: Can't control screen brightness on Toshiba l650-11f

Check to see that you have the latest BIOS Revision, brightness control was fixed with revision on some models