AMD VISION Engine Control Center cannot be started. S855D-S5120

Reply
Member
Posts: 6

AMD VISION Engine Control Center cannot be started. S855D-S5120

[ Edited ]

When trying to open the AMD VISION Engine Control Center I get the folling message, "AMD VISION Engine Control Center cannot be started. There are currently no settings that can be configured using AMD VISION Engine Control Center."

 

I've just bought this computer new and was able to access the AMD VISION ECC for the first few days. Suddenly, I can no longer access it.

 

I tried to update the drivers from the Thoshiba support page. Now I get this message, "AMD Catalyst Control Center cannot be started. There are currently no settings that can be configured using AMD Catalyst Control Center." Almost the same message as I got the first time.

 

EDIT: I forgot to provide my graphics information. The Laptop has a AMD A10-4600m with HD 7660g integrated graphics.

--
Toshiba Satellite S855D-S5120: AMD A10-4600m, HD 7660g, 8GB DDR3 1600MHz
Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

[ Edited ]

Is THIS the display driver you installed? Even if yes, please try again.  It is AMD Display Driver Version  8.982.7 dated 11/02/12.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 6

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

Before I was aware of your post I reset the computer to factory settings. After the factory reset was complete the AMD VISION Engine Control Center worked! However, after I closed the AMD VISION Engine Control Center, I tried to open it again and I got the same error message.

 

IMPORTANT NOTE: This is happening even though I have made no changes to the system; I haven't deleted programs, haven't updated anything, haven't even been on the internet, yet, the program wont open.

 

After it failed again, I saw your post and did as your instructed. I downloaded the driver and attempted to install the driver. The driver extracts itself but no setup occurs after the extraction.

--
Toshiba Satellite S855D-S5120: AMD A10-4600m, HD 7660g, 8GB DDR3 1600MHz
Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

I'm at a loss also, robinson. The reset to out-of-box should have fixed it and it did.  Very puzzling why the fix didn't hold.  Maybe someone else will come up with some ideas.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 46,808
Topics: 83
Kudos: 8,807
Solutions: 3,146
Registered: ‎12-04-2008

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

 

Satellite S855D-S5120

 

Downloads here

 

 

Seems to be a common difficulty.

 

   "AMD VISION Engine Control Center cannot be started. There are currently no settings that can be con...

 

What happens after you upgrade to Windows 8.1? It requires a different driver.

 

   How to Update from Windows 8 to Windows 8.1

-Jerry
Channel 9
Member
Posts: 6

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

+1 Jerry_Lippey

 

After following these instructions exactly, How to Update from Windows 8 to Windows 8.1,  everything works great.

 

Thank you both for your time.

--
Toshiba Satellite S855D-S5120: AMD A10-4600m, HD 7660g, 8GB DDR3 1600MHz
Posts: 46,808
Topics: 83
Kudos: 8,807
Solutions: 3,146
Registered: ‎12-04-2008

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

Good news!

-Jerry
Channel 9
Member
Posts: 3

Re: AMD VISION Engine Control Center cannot be started. S855D-S5120

I am having the same issue, I have a L775D-S7223 and cannot get anything to work

I am at the point now that I will be throwing this POS against the nearest wall in about 10min.