I own a Toshiba Satellite A205-S6806 laptop that I recently upgraded from the default operating system install of Vista to Windows 7 (32 bit). During the upgrade, I was able to successfully install all of the Windows Updates but one caused me problems, specifically a display upgrade for the Mobile Intel(R) 965 Express Chipset Family Driver (I was unable to determine the Microsoft KB number for the update). When I reboot, the display assumes a very low resolution and the touchpad becomes disabled. Through use of the keyboard as a mouse, I was able to enter the Device Manager and observe that the touchpad driver had a "code 10" with all the driver options (UPDATE DRIVER, DISABLE, UNINSTALL, etc.) grayed out. I rolled the restore point back before this update, hide the update, and disabled Automatic Updates until I resolved this problem.