TV will not turn on but has a blinking green power light

Reply
Member
Posts: 1

TV will not turn on but has a blinking green power light

i have a TOSHIBA 32" LCD TV (32AV502R) and it will not turn on.  I have tried using the remote and the power button on the side of the TV.  I unplugged the TV yesterday for most of the day.  Today, i have plugged it back in and the little green light on the front of the TV under the word POWER just flashes.  I am not getting response from the unit.  Any guidance would be greatly appreciated.  Is it time for another TV?

Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: TV will not turn on but has a blinking green power light

It sounds like it needs servicing. I'd suggest contacting customer support at (800) 631-3811.

- Peter
365
Member
Posts: 2

Re: TV will not turn on but has a blinking green power light

MINE is doing that exact thing !!!! I have no idea what is up ...arrgghh sorry couldn't help, i'm looking for help myself

Member
Posts: 1

Re: TV will not turn on but has a blinking green power light

I just in boxes the same tv. Bought it 2 yrs ago, worked well, used in only 6 mnths, now I too have the same issue. No answers. We should note that this TV is built with the Samsung screen LTA320apo1. Thinking there must be a conflict within the power and the screen? Any know how to fix this yet?