LED 42" Toshiba Regza SL836 - volume increasing itself

Reply
Member
Posts: 1

LED 42" Toshiba Regza SL836 - volume increasing itself

Hello there, I got a problem with my Toshiba TV... The volume is increasing itself which is sooooo annoying. It does it randomly, I tried to remove the batteries of the RC - still increasing alone. So it's not from the RC. In fact when I catch it doing that I`m trying to lower the volume from the RC and it stucks to one position and doesn't go up or down, like someone is pressing the V+ sensor button on the TV. Tried to clean the sensors on the TV - without effect. If anyone knows the reason, or better - the solution of that, because it's really annoying, and I really like that TV, and it's almost new (bought it before 4-5 months)... Any thoughts are appriciated!

Posts: 21,514
Topics: 69
Kudos: 788
Solutions: 480
Registered: ‎10-04-2011

Re: LED 42" Toshiba Regza SL836 - volume increasing itself

That model doesn't appear to be from the US, so I don't have any information on it. You may want to contact Toshiba in your region. However, you may want to physically block the sensor on the TV the next time it happens. If the problem persists, you'll be ruling out some other device interferring.

- Peter