How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

Reply
Member
Posts: 1

How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

My remote turns up the TV volume along with the soundbar. I need to disable the TV speakers. Thanks.

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

You need to simply lower the volume all the way.

- Peter
Occasional Contributor
Posts: 46

Re: How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

Peter that is completely incorrect.

 

It depends on how you have the soundbar setup.  There are settings to disable the speakers in the "audio" menu.  If you have it set up via HDMI, you can also press the quick button on your remote and change the setting from tv speakers to amplifier.

 

 

 

 

Member
Posts: 2

Re: How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

Settings of what? TV or Soundbar. I use Optical cable. Any way to turn off the TV sound? My TV model is 40E220U

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: How do I disable the Built-in speakers on a 46SL417U? Want to use a soundbar.

On that model, the speakers can only be disabled if using an HDMI audio system as far as I know. When using an optical cable, you'd need to turn down the speakers on the TV.

- Peter