"No Video Signal" message on TV

0 Kudos
Started ‎02-25-2013 by
Modified ‎04-25-2013 by
(21,383 Views)

If the "No Video Signal" message is displayed on the TV screen, check the following:

 

  • External devices are connected properly.
  • The TV is set on the correct input for the connected device.

Refer to the following Knowledge Base articles for complete information on properly connecting and setting the TV input:

 

 

Contributors