|
|
|
07-07-2011
03:38 PM
- last edited on
07-10-2011
03:25 PM
by
jim
Well I am composing this message on my Thrive tablet. Purchased on Naval base 1 July. Guess since I'm one of the first to get one I will be the first to post a problem. When I leave the thrive in stand by and press the power button it fails r To come on and requires rebooting. Just a small quick but annoying.
Solved! Go to Solution.
07-08-2011
12:53 PM
- last edited on
07-10-2011
03:25 PM
by
jim
I think you will find this link helpful regarding standby/power button.
http://forum.xda-developers.com/showthread.php?t=1
Also, this forum is thrive-dedicated. http://www.thriveforums.org/forum/forum.php
Hopefully Toshiba Support is reading this.
07-10-2011 04:47 PM
I have the same problem with my 32GB tablet. This is a pretty serious and large oversight. Toshiba needs to come clean fast about the fix. After the battery swap suggested on the other site, I can make the tablet come out of sleep, but I don't have any way of logging back in...I only see a time/date in front of a backdrop.
07-11-2011 03:12 PM - last edited on 07-13-2011 02:19 PM
I've forwarded the problem reports to technical staff for evaluation. Meanwhile, it's worth noting that user ryanp0617 at the xds-developers.com forum link above posted this workaround there:
"I fixed it by taking out the battery plugging in the tablet turning it on with no battery, then I put the battery back in and unplugged the device while it was still on it immediately noticed the battery and the sleep problem stopped happening hope this helps."
Don't know if that's a 1-time permanent "fix" but that user posted his message on 7/5 and has not since posted an update stating that the problem has returned. (Btw, I don't know how he got his hands on a Thrive on or before 7/5.)
UPDATE: Many have reported the above-mentioned workaround to be ineffective as a solution to this issue, so I'm no longer comfortable asking everyone to give it a shot.
Jim
07-11-2011 10:46 PM
Having the same issue.
Unfortunantely, Jim's recommended fix didn't work. Seemed to work fine when I press the power button to put it to sleep manually and wake it up, but after awhile, even that stops working. I set the tablet to go to sleep after 30 minutes and it goes to sleep much sooner than that (like less than 5 minutes). And then I can't wake it up again. Seems to have a mind of its own. Hope Toshiba has a fix for this problem soon.
07-12-2011 05:43 AM
jim wrote:I've forwarded the problem reports to technical staff for evaluation. Meanwhile, it's worth noting that user ryanp0617 at the xds-developers.com forum link above posted this workaround there:
"I fixed it by taking out the battery plugging in the tablet turning it on with no battery, then I put the battery back in and unplugged the device while it was still on it immediately noticed the battery and the sleep problem stopped happening hope this helps."
Don't know if that's a 1-time permanent "fix" but that user posted his message on 7/5 and has not since posted an update stating that the problem has returned. (Btw, I don't know how he got his hands on a Thrive on or before 7/5.)
Jim
Thanks for forwarding sleep problem to the tech guys. Hopefully this can be corrected with a firmware update. Btw, the Australian market had earlier access to the Thrive, so the mentioned user may have originated from there.)
07-12-2011 07:35 AM
I have had this issue on two 16GB versions. This is the only major bug I have found so far, and hope it get fixed soon.
07-12-2011 08:06 AM
Samething has been happening to me, I tried the work around and also a factory reset. Neither worked.
Hopefully Toshiba will fix this soon, this has been the only issue I've had with the Thrive so far.
07-12-2011 08:48 AM
Glad you let us know that the factory reset didn't work. Almost did that last night, but even a SD card backup won't restore everything to the way it used to be and I spent a lot of time on downloading apps and app placement. Really don't want to have to do that again.
Hopefully Toshiba addresses this quickly.
07-12-2011 11:20 AM - last edited on 07-13-2011 02:22 PM
If you are experiencing the subject issue with a Thrive tablet purchased in the US please send me a Private Message with the following info:
Click here to send me a Private Message.
Please stay tuned to this message board topic. I will post any updates I receive on the issue right here.
UPDATE: Please see this message for a possible workaround.
Thanks,
Jim
[ Edited to add bullet for Thrive base memory ]
07-12-2011 11:36 AM
PM sent.
Thanks a lot Jim
07-12-2011 12:47 PM
PM sent. Thanks, Jim.
07-12-2011 03:13 PM
07-12-2011 04:58 PM
PM sent. This is starting to be unbearable.
07-12-2011 05:00 PM
07-12-2011 05:38 PM
07-12-2011 05:43 PM
I can confirm that this happens even with the power cord plugged in.
07-12-2011
07:02 PM
- last edited on
07-13-2011
11:05 AM
by
jim
My Toshiba Thrive arrived today and upon turning it on it stays on the android flash screen and doesn't boot up?
[ admin edit of subject ]
07-12-2011 07:26 PM
I had the Thrive since yesterday & had it plugged in overnight. Alarm did not turn on the next morning & had to force a reboot.
07-13-2011 05:13 AM
|
Copyright © 2011 Privacy Policy | Terms of Use | Forum Terms of Service | Contact Us Feedback
|
|