SD card max size

Reply
Member
Posts: 2
Accepted Solution

SD card max size

Just ordered my Thrive 32G to replace an aging Toshiba Satellite laptop.  I have read conflicting posts on the Max SD card size.  I've read posts claiming anywhere from 32G to 128G.  So just what is the max card size to use?

Thanks!

Regular Advisor
Posts: 374

Re: SD card max size

128GB is the max size it will handle.

Paul L. Dale
**********************************************
Thrive Developer - ThriveForums.org

View solution in original post


All Replies
Regular Advisor
Posts: 374

Re: SD card max size

128GB is the max size it will handle.

Paul L. Dale
**********************************************
Thrive Developer - ThriveForums.org
Member
Posts: 2

Re: SD card max size

Thanks for the answer.  Will look into a 128G card.

Member
Posts: 6

Re: SD card max size

Hello all. If 128G is the max size of an SD card, does it need special formatting such as exfat? Or other?
Member
Posts: 1

Re: SD card max size

[ Edited ]

Spoke to tech support.  They say 64gb is the largest the thrive will read.  You have used a 128gb without any problems?  It reads and writes OK?