02-18-2012 12:04 PM - edited 02-18-2012 12:08 PM
02-18-2012 10:02 PM
Toshiba Admin,
I'm also interested in the upgrade to Android 4.0. Please provide the Thrive owners with an estimated release date for Ice Cream Sandwich.
Thank you,
-K
02-20-2012 12:43 PM
Just hear today (Feb. 20th 2012) that Acer is pushing out ICS for their Ionia A200Tablet, The 7" A100 and the 10" A500 Tablets will get their updates around April.
This is good news for the Acer community but does little for those of us who are left salivating at what other manufacturers have already begun to provide for their customers.
On the bright side Toshiba was also late with the 3.2 release, when compared to the rest of the industry so we will have to wait, perhaps we might see it in July or August time frame.
02-20-2012 03:46 PM
02-21-2012 10:19 AM
A few minutes ago on Twitter, @ToshibaUSA tweeted...
"We are targeting the end of Spring for ICS availability on the Thrive 10-inch."
That's the latest.
Jim
02-21-2012 12:25 PM
Thanks for passing that along Jim. Not all of us follow anything on twitter!
02-24-2012 03:34 PM
Can we expect to see the ability to save apps to the SD card on the Toshiba Thrive with the ICS upgrade?
02-25-2012 08:37 AM
wait worth waiting for!
02-26-2012 02:59 AM - edited 02-26-2012 10:33 AM
02-26-2012 10:23 AM - edited 02-26-2012 10:29 AM
Word is that Toshiba will be releasing an update to ICS for the Thrive late in the spring . See this page for additional information:
http://blogs.computerworld.com/19766/toshiba_thriv
Since I'm a newbie when it comes to the Android OS, I'm going to be patient and wait for the upgrade.
02-28-2012 09:38 AM - edited 02-28-2012 09:41 AM
02-28-2012 02:52 PM
dash: you said: "I am currently not even seeing an update for 3.2 on my Service Station . . . I hope I will be able to see ICS when it is available."
Are you saying you are not updated to version 3.2? If not: 1. are you here in the USA? If so, did you buy your Thrive from WOOT? If so go to the other forum and get the update (non-rooted version) that will allow you to get version 3.2 because until you do, you will not be able to update to ICS
03-01-2012 08:39 AM
03-01-2012 12:44 PM
03-01-2012 01:09 PM
This is AWESOME, NOT!!! The 2/28/12 update broke my thrive..won't boot now. I'm sure support's fix will be to wipe clean ![]()
03-04-2012 09:37 AM
03-05-2012 02:01 PM
-dash-,
To clarify for the benefit of others, what I said is that "Yes, Toshiba Service Station OTA updates published by Toshiba in the US for your [US purchased] THRiVE will be delivered anywhere in the world over the Internet."
This is based on info you provided that your tablet was purchased in the US.
So the key point is that updates for US-purchased Thrive tablets are available to those tablets from any physical location. Updates for US-purchased Thrive tablets will not be available for tablets purchased in other regions (even if they are physically located in the US.)
Jim
03-06-2012 04:36 AM
-dash-
My 16gb Thrive (stock,purchased in the US)is also only showing the one update: HC 3.1.01.5.0032 to 3.1.31.5.0011. I haven't received any other since this one dated Oct 2011. My THRiVE is encrypted and nobody has given me a satisfactory answer as to why the update won't go ahead, but gives the message: 'An error has occurred copying the system image file'. There MUST be a better way than the, often suggested, factory reset??!!
Hope I can get the ICS(when it finally arrives) and bypass 3.1.31.5.0011.
03-06-2012 08:03 AM
Rodster, you said: " My 16gb Thrive (stock,purchased in the US)is also only showing the one update: HC 3.1.01.5.0032 to 3.1.31.5.0011. I haven't received any other since this one dated Oct 2011. My THRiVE is encrypted and nobody has given me a satisfactory answer as to why the update won't go ahead, but gives the message: 'An error has occurred copying the system image file'. There MUST be a better way than the, often suggested, factory reset??!!"
Go here for your answer: http://forums.toshiba.com/t5/THRiVE-Tablets/How-do
03-07-2012 02:21 AM
Jim,
If thats the case why am i not seeing any upadtes other than 3.1.01.5.0032 to 3.1.31.5.0011?
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.