3.2 Problems

Reply
Occasional Contributor
Posts: 11

3.2 Problems

I just installed 3.2 and have seen some odd results.

 

1) When hooked to my computer via usb every directory shows up twice.  For example there are 2 "Movie" directories.  There are now 4 "dowbnload" directories ( 2 starting in lower class "d", 2 starting with uper case "D")

 

I copies a movie over and go into the Toshiba media player and the movie is listed 2 times even though there is only 1 copy on the tablet.


Member
Posts: 4

Re: 3.2 Problems

The issue is they have remapped the SD card in the update to a new location you need to have the media rescanned to find its new location. To do this go you the market and install one of the free rescan apps - search rescan to find one. This will cause the media player to reload its cached media. This should solve your problem.
Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: 3.2 Problems

Someone reported something similar. Take a look at his message and see if that works for you!

- Peter
Occasional Contributor
Posts: 11

Re: 3.2 Problems

NO, this has nothiong to do with the SD card  This is internal memory.  Did you look at the attachmernt? No.

Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: 3.2 Problems

Yes, I looked at the attachment.

 

I also see no mention of the SD card in the post to which I linked.

 

Did you try the fix?

- Peter
Member
Posts: 2

Re: 3.2 Problems

[ Edited ]
I experienced 2 problems with the update:

1 - BOOT UP TIME TAKES SEVERAL MINUTES that i have to leave it for sometime to complete the process.

2 - FILE MANAGER TAKES TOO LONG to be useable with the ff warning: THE SYSTEM IS SCANNING FILES. FILE OPERATIONS ARE NOT PERMITTED AT THIS TIME whenever sd card or usb flash drive is inserted