Don't know when this happened but the pictures in gallery that are synced from Picasa web are now blank. The thumbnail squares are blank, the Picasa icon is on the stack, the album names are there but the pictures are blank. The images are fine on the web. Turning sync off then on does not fix it. I know they were there in the past and I can't be sure if 3.2 caused this. I think the only way to correct this is to remove the albums from the web, sync will remove from gallery, then upload again to the web. Any other ideas. p.s. Does anyone else feel like a they are testing a Beta product with these **bleep** Android tablets?