error F3-FF00-0006

Reply
Member
Posts: 1

error F3-FF00-0006

my father brought me the toshiba satellite L500 for christmas and upon opening the notebook a message of a recovery partition for windows 7 occured. I answerec it to be installed with the 64bit and several questions later it began to install, however after about 20% into the installation an error of F3-F200-0003 errupted. I decided to call the toshiba service line which informed me i mmust restart my notebook and hold down the "0" key for three seconds, after doing so another error message occured called F3-FF00-0006. I've also tried reboot the system defaults but that also led to nothing please please help i have run out of ideas and really need my laptop for university....

 

Member
Posts: 8

Re: error F3-FF00-0006

seems like an issue with the hard drive

Member
Posts: 1

Re: error F3-FF00-0006

I'm facing the same problem, i also bought the laptop before Xmas....but now i'm in Brasil and i can't change it....