Wipe computer clean

Reply
Member
Posts: 5

Wipe computer clean

I want to clean my a105-s2071 laptop. I want to clean it to start over for my kids to have. Do I do a factory reset or something else. Any help is great. Right now I think I need to do a factory reset.
Occasional Contributor
Posts: 12

Re: Wipe computer clean

Reinstall using Toshiba re-installation media.  Insert re-install media in CD/DVD, answer what type of re-install is desired and wait.  The process is simple if you have the re-install disks. 

Posts: 47,516
Topics: 84
Kudos: 9,033
Solutions: 3,200
Registered: ‎12-04-2008

Re: Wipe computer clean

 

Satellite A105-S2071

 

If you don't have the recovery discs, you should be able to order them from Toshiba.

 

   Order Toshiba Recovery Media

-Jerry
Channel 9