Windows has detected a registry/configuration error

Reply
Member
Posts: 1

Windows has detected a registry/configuration error

I haven't used my Protege 3110CT in many years.  When I start to boot up I get the message:

Warning: Windows has detected a registry/configuration error. Use SCANREG to correct this error.

 

However, I cannot get into DOS to do a SCANREG nor do I know any other method.

 

I do not have any of the startup disks.

 

My machine has Windows ME on it.

 

I do have an external floppy drive and CD drive.

 

Any assistance is appreciated.

 

Bob

Posts: 48,000
Topics: 85
Kudos: 9,137
Solutions: 3,234
Registered: ‎12-04-2008

Re: Windows has detected a registry/configuration error

 

Portege 3110CT 

 

You can download a bootable DOS floppy here.

 

   http://www.bootdisk.com/bootdisk.htm

 

If you can locate a download of Scanreg.exe, then boot to DOS and run scanreg /restore to
go back to a previous known working copy of your Windows Me registry.

 

Maybe this one works (I don't know).

 

   http://www.mesich.com/download/SCANREG.EXE

-Jerry
Channel 9